Part Number: TUSB320LAI
Other Parts Discussed in Thread: TUSB320
Tool/software:
Hi,
Our product utilizes the TUSB320LAI CC controller to manage USB-C port behavior. In accordance with the EU Common Charger Directive, we are required to comply with EN IEC 62680-1-3.
Recently, we encountered several test failures during IEC compliance testing in SNK mode and would appreciate your support in identifying a solution.
The test failures are as follows:
-
TD 4.3.1 Sink Connect Source Test – The PUT does not assert Rd on the CC pin.
-
TD 4.3.2 Sink Connect DRP Test – The PUT, when acting as PUT_R, does not assert Rd on both CC pins.
-
TD 4.3.3 Sink Connect Try.SRC DRP Test – The PUT, as PUT_R, does not assert Rd on both CC pins.
-
TD 4.3.4 Sink Connect Try.SNK DRP Test – The PUT does not maintain Rd on both CC pins for the duration of the test.
-
TD 4.11.2 Sink Dead Battery Test – The PUT improperly asserts Rp, which is not allowed.
Below is the schematic snippet for the CC controller. Please note that the port’s default role is configured as DRP. However, for testing purposes, we set the port to UFP (unattached.SNK) via I²C. The I²C configuration values used are:
30 32 33 42 53 55 54 00 00 30 10
However, based on the test results, it appears that the port role was not successfully switched from DRP to SNK mode.

Regards,
Jeff