Part Number: DP83867CR
Tool/software:
Hello E2E Experts,
Good day.
Using center tapped magnetics, what specific compliance did the part failed?
Is is EMC? Or something else.
Regards,
TICSC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TICSC
Can you please provide more context for this question? Is the customer seeing a particular EMC failure with the DP83867CR? If this is the case, then can you please share the compliance report?
Thanks
David
Hello David,
Good day and apologies for the confusion.
I am planning to use RJ45 with integrated magnetics.
Based on the link:
DP83867CR: Ethernet Connectors with integrated magnetics
Center-tap magnetics shorted together creates compliance issues.
What specific compliance? Or perhaps certifying body?
On the other hand, the DP83867 EVM uses magnetics center tap shorted together which is contradicting to the post.

Regards,
TICSC
TICSC
Shorted center taps can increase the common mode noise on the MDI lines, increase cross talk between TX and RX, and also affect the bias voltage point on TX. It can impact the Direct Contact Discharge ESD, EFT, and Surge performance.
As you can see from the below drawing, the short tap of the transformer on the EVM is not shorted together.

Thanks
David
TICSC
You can use this integrated transformer. But typically we see discrete magnetic has better EMC performance than the integrated magnetic.
Thanks
David