Part Number: TMUXHS4412
Tool/software:
I'm trying to reply to my old post, but I'm getting the error "Your posting frequency has exceeded allowed rates. Please wait 1 minute(s) to post again."
I can only create a new question to reply to my previous discussion.
"Dear Katy,
Thank you so much for your reply.
Unfortunately, the scope it was used to measure the signals is a simple scope 50MHz 1GSa/s from the client, so we don't have much more information about the LVDS signal, like the operating frequency, also.
Just to be sure, the TMUXHS4412 can handle a maximum signal voltage of 2.4V, with a peak-to-peak of 1.8V, correct? That is, the maximum common-mode value it can support is 1.5V if the peak-to-peak value of the signal is 1.8V, correct?
Best Regards!"