Part Number: TUSB322I
Other Parts Discussed in Thread: TUSB322, TPS25751
Tool/software:

Can I able to achieve USB type c PD 3.0 configuration from the design mentioned above ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm designing a USB Hub for drone application . In that USB Type C with PD 3.0 is the one of the output port .
Can you suggest any PD controller to achieve this ?
Hi Supriya,
The TUSB322 allows for 5V 3A (15W) maximum sourcing and sinking of power for charging. The TUSB322 does not support any USB-C alt. modes.
PD typically allows for high charging voltages. PD support alt mode as well. If you do not need the extra functionality for PD, and just need to detect the USB-C orientation and source and sink up to 15W of power, then the TUSB322 will be fine.
If you need to have the PD functionality I will reassign this ticket to the PD team.
The power requirement is 15W-87W for PD port . So I request you to reassign this to PD team