This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: When using the external ref clk of the serializer DS90UB941 with a 15-inch large screen DS90UB948 deserializer, the screen displays abnormally and has water ripple

Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: LMK3H0102

Tool/software:

For some information, please refer to the ticket below. Our ref clk source is LMK3H0102 clock chip.

LMK3H0102-Q1: How to read the chip address through I2C in OTP mode and then configure it to I2C mode - Clock & timing forum - Clock & timing - TI E2E support forums

In addition, we have two screens. The deserializers are DS90UB948, one 12.9-inch and one 15-inch screen, but the 12.9-inch screen display is normal, and the 15-inch screen display is abnormal. Please help analyze the reasons for the abnormal display of 15-inch screen from the perspectives of DS90UB941 and DS90UB948. Thank you.