This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXCH8T245: Can you tie multiple inputs/outputs together to increase current drive?

Part Number: SN74AXCH8T245


Tool/software:

Hello,

Can I connect several outputs of SN74AXCH8T245 together if I also connect the corresponding inputs together? I am hoping to get more drive strength than 12mA. I cannot use the equivalent LXCH device because one of my voltage rails is below 1.1V.

Thank you!

Best regards,

Zach Kimble