This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVCP22: Connection when OUT pin is not used.

Part Number: SN65LVCP22

Tool/software:

Hi Team,

Hello team,

I am designing a circuit using the SN65LVCP22.
In this case, only OUT0 is used, and OUT1 is not used.
At this time, is it okay not to connect anything to OUT1, or is some termination required?

In this case, EN0 is fixed to High, and EN1 is fixed to LOW. LVDS signals are input to IN0 and IN1.

Regards,
Konoha