Part Number: TDES960
Other Parts Discussed in Thread: AM68A,
Tool/software:
Body:
Hello TI Community,
I am developing a custom board based on the AM68A (AM6852ATGGHAALZR) reference design. My goal is to interface three cameras using Arducam’s V3Link D-CH adapter and TI’s TDES960 deserializer.
I attempted the following configuration:
-
Connected three cameras to a single Arducam V3Link adapter board.
-
Used TS3DV642A0RUAR to switch CSI lanes between the TDES960 and AM68A SoC.
-
However, in this setup, I was unable to stream all three cameras in high-resolution mode reliably.
Then, I tested a modified configuration:
-
Connected two cameras to one Arducam adapter, and the third camera to a separate Arducam adapter (with a second TDES960).
-
This setup worked properly in high-resolution mode.
I have attached the schematic showing the interfacing between TDES960, TS3DV642A0RUAR, and the AM68A CSI2_RX ports