This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA6408A: VIH, VIL, VOL VALUES of the SC0-7, SD0-7 ports of the TCA6408APWR IC

Part Number: TCA6408A
Other Parts Discussed in Thread: TCA9548A

Tool/software:

im using the  TCA6408APWR with 1.8V VCC, 1.8V I2C on the SDA, SCL pin (VDPUM ) and using 8 i2c output ports with 1.8V and 3.3V. 

what is the SD, SC ports VIH, VIL, VOL values for 1.8V level and 3.3V level. can i use different i2c bus on the TCA6408A IC with different supply. i need the DC analysis values.