Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: PCA9306 Vrerf 1.2V-> Vref 0.9V operation's verification

Part Number: PCA9306

Tool/software:

Hi Team, 

     There is a question for PCA9306, on datasheet recommendation, VREF1 supports 1.2 V to VREF2 - 0.6 V, and VREF2 must be between VREF1 + 0.6 V to 5.5 V. If VCC1 = VREF1 = 1.26V. VREF2 = 1.26V + 0.6V = 1.86V. 

However, on customer side board, they found that PCA9306 can support 1.2V(Vref1) to 0.9V(Vref2) level transmission. Could you please explain why the voltage on Vref2 can be lower than Vref1?

please refer to the following