Part Number: DP83826I
Tool/software:
I will be using 100Base, full duplex.
With an IC with the same specs as the DP83826I I was using previously, TD+, TD-, RD+, and RD- were pulled up with 49.9 Ω as shown in the diagram below.
Is this unnecessary with this IC? Also, is the 10pF multilayer ceramic capacitor (not installed) on the same communication line unnecessary?