This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD1E0B04: Is there a s-parameter model for this TPD1E0B04 (DPL)?

Part Number: TPD1E0B04

Tool/software:

Hi TI support,

We are working on investigating the capability of implementing this TPD1E0B04 (DPL) in our high-speed ASIC design. We are targeting 10GHz-20GHz application. We would like to ask if there is an s-parameter model for this TPD1E0B04 (DPL) so that we can do the insertion loss and capacitance simulation? 

Also, 6 months ago we have requested a Spice model of the same TVS diode, but the leakage current result @ 3.3V is far off compared with the datasheet. Do we need to request small signal model in addition to it, if we need to model the leakage also? Not sure if the Spice model we are given is only good for DC simulation with large signal. If there needs additional model for the small signal simulation, we would like to request it also besides the s-parameter model.

Thanks for your help.

Best,

Lixian

  • Hi Lixian,

    Yes, s-parameter files are available on TI.com for the DPL version, I have also attached here.

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/138/TPD1E0B04DPL.S1P

    What is the leakage current you are seeing? We don't have any small signal simulation models available for this device outside of the PSPICE model and s-parameter file.

    Best Regards,

    Josh Prushing