TCA9548A: Can I put the TCA9517 in front of the TCA9548?

Part Number: TCA9548A
Other Parts Discussed in Thread: TCA9517

Tool/software:

Hello E2E Experts,

Good day.

Can I install the TCA9517 in front of the TCA9548? Both resistors in the pull-up configuration are set to 2KΩ. Would this arrangement cause any issues? My hardware circuit has been experiencing IIC device scanning failures after program modifications – whereas it worked perfectly before changes. Could this instability be caused by the series connection between the 9517 and 9548 components? How can I resolve this issue?

Regards,

TICSC