This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUXHS4212: Cascaded implementation

Part Number: TMUXHS4212

Tool/software:

Hello Team,

Could you please help to review the schematic of the cascaded implementation which was communicated previously with Blok diagram?

TMUXHS4212_cascaded_Implementation.pdf

Kindly confirm the requirement of coupling caps on Tx side of both MUXes.

But we got a very low bandwidth of ~100Mbps, when performing below test.

We performed both sequential and random read/write tests using fio with direct I/O.

The device used to test the interface was Sabrent 512GB Rocket NVMe PCIe M.2 2242 SSD.

Test Setup Summary
--------------------------
Tool: fio with libaio engine and direct I/O
Block Sizes: 1M for sequential, 4k for random
Device: Sabrent 512GB Rocket NVMe PCIe M.2 2242 SSD
Mount Point: /mnt/PCIe

Please help.