Part Number: TUSB320HAI
Other Parts Discussed in Thread: TUSB320
Tool/software:
I am facing USB C-to-C compatibility issues with some laptop brands. I am using the TUSB320HA device with the Port pin left open to select DRP mode by default. I am experiencing the following issues when attempting a USB C-to-C connection to a laptop:
- No connection made, the laptop does not detect the USB connection. TUSB320 register 0x09 also shows no attachment.
- For some laptop brands, the TUSB320 register 0x09 shows it attached as DFP SRC while the laptop has not detected the USB connection.
- For some laptops, the TUSB320 device successfully attaches
I have tried placing the TUSB320 device in UFP mode using I2C, but the behavior still remains the same. This connection issues are not observed when using a USB C to USB A connection. A power cycle also resolves the issue, the TUSB320 device attaches a USB C-to-C connection if the cable is connected before power is switched on.