Part Number: TCA39306
Hello team,
I have some questions about I3C. TCA39306 will be used to change the voltage between 1.8V and 3.3V and speed is 12.5MHz.
- TCA30306 have 12.5pF max of ON capacitance for SDAn. Does this mean both SDA1 and SDA2 have 12.5pF max and total parasitic capacitance at SDA is 25pF?
50pF is the max bus cap value that MIPI defined so just another 25pF is allowable bus capacitance? - Is there formula to decide suitable pull up resistor value?
Best regards
koyo