Part Number: DP83867E
Hi experts,
My customer is looking for an ethernet PHY which can support following requirements.
- 1000BASE communication through RJ-45
- SGMII
- No MDIO connection
Below is my questions.
- When I see DP83867E datasheet, it can support all of the three requirements by using auto-negotiation and appropriate strap configuration, is it correct?
- As customer does not use MDIO/MDC pins, what is the recommended termination? It seems general recommendation is to pull them down. Any recommended pull-down value?

3. What is the strap configuraiton needed to achieve the three requirements above? Below is my understanding and questions.
- RX_D0, RX_D1...Depending on PHY Address customer wants to use. RX_D0 and RX_D1 must have the same strap configuration
- RX_D2, RX_D3...Same as RX_D0, RX_D1
- RX_CTRL...MODE 3 to enable auto-negotiation
- GPIO_0/1...Any requirements?
- LED_2...Any requirements?
- LED_1...Any requirements_
- LED_0...SGMII enable must be 1 (MODE 2 or MODE 4)
Regards,
Kento