DP83640T-EVK: Can use this eval kit as standalone system for my FPGA ?

Part Number: DP83640T-EVK
Other Parts Discussed in Thread: USB-2-MDIO, MSP430F5529

I have bought this DP83640T evaluation kit. I am using FPGA for time-stamping and synchronisation. I would like to your help with regards to a few things.

1. I want a pps aligned for which i intent to use the my FPGA GEM routed through PL to the DP83640T. Programm it through MDIO and get the pps into my PL. I can use GMII (uses 8 data bits) ? (I am planning to use only lower 4 bit [3:0] ) so i can so with the MII interface of the DP83640T (which it seems compatible with mentioned in the datasheet) ?

2. I can see a second chip on the eval kit. From the schematic capture it seems like a micro-controller ( CY7C68013A-56LFXC) is also used inside . I would like to know Can i programm this micro-controller to make the evaluation kit be used as a standalone system for programming the PHY chip to give me a PPS signal ? 

3. If 2nd is true . I can use CCS for it or do i need a specific software to programm it or go bare-metal C on it ?