This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9543A: Regarding the Tj specification of TCA9543APWR

Part Number: TCA9543A

Hi Team,

Regarding the Tj specification of TCA9543APWR
The datasheet only specifies Ta = 85 °C and does not indicate Tj.
The customer would like to confirm whether Tj can be higher than 105 °C.
Please provide the Tj (junction temperature) specification.

Thanks

  • Hello Allen,

    The Tj of our multiplexers can be calculated by following this FAQ.

    According to my calculation Tj max comes out to be 92.3C. 
    While it is a calculated a spec which is an approximation I cannot recommend the customer to exceed it. 

    Thanks,

    Nir