Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD451: Using ESD451DPLR for GNSS antenna protection

Part Number: ESD451

Hi @ti team,

Currently we are planning to use ESD451DPLR in the GNSS antenna path near to the on board UFL connector to which a 3.3V supported active antenna is going to get connected. Can you please let me know whether this diode is suitable for the same. 

  • Hi Sai,

    Short answer is yes, this diode is suitable.

    The 3.3V is lower than the diode VRWM. I would also look at the insertion loss graph just to make sure this is okay. Insertion loss is low for the frequencies GNSS use (around -2.5dB). Look at the graph below. 

    Let me know if you have any questions.

    Best,

    Bryan