Part Number: DP83826I
If the DP83826(A) is used with the Beckhoff EtherCat IP-Core the Beckhoff PHY Addendum
Beckhoff wants that MI link detection is disabled if IP-Core 3.xx Version is used, because this Version is making write accesses to PHY register 9.
What exactly happens if IP-Core 3.xx with activated MI link detection is used with DP83826(A)I (enhanced mode). Which bits are changed in this Register?
Kind Regards
Thomas