This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD2450: Recommended biasing resistors

Part Number: THVD2450

Hallo together,

we referencing to the this question in the forum: THVD2450: idle bus failsafe issue - Interface forum - Interface - TI E2E support forums 
do we need biasing resistors for having a true failsafe?
If yes, could you please recommended us the biasing resistors for the THVD2450 when we need to have the transceiver as true fail-safe receiver?

Best regards,
David CONDOR

  • Hi David,

    Thanks for reaching out on E2E!

    For that E2E post you are referencing, Parker's comment highlighted in green is the way to go.

    So if you want true failsafe for THVD2450, you can add resistors to the bus lines. Just note that you want to keep the overall bus impedance matching, and adding the failsafe resistors will affect this. 

    This app note explains it in full detail, but you can just use this equation:

    Here R_T2 is the termination resistor at that particular node, and R_FS is the failsafe resistors (multiplied by 2 for both the pullup and pulldown resistor). Also keep in mind that if you have multiple failsafe resistors on the RS-485 bus, these would technically be in parallel. So you will want to increase the R_FS value for each node that has biasing resistors. For example, if you have 3 nodes with failsafe resistors, then you will need each node to have 3*R_FS resistance. 

    Let me know if that makes sense.

    Best,

    Ethan