Part Number: TUSB2077A
I am designing a 20 port USB hub to expand the capabilites of a host controller. I have attached the USB hub portion of the schematic for a review, if possible.
The hub is self powered by a 5V, 4A capable wall adapter.
The 20 USB devices will be permanently installed, and as such will be already inserted when the board powers on.
Average current draw of the USB devices is 20mA, with short spikes up to about 200mA once every few minutes.
Thank you very much for all your help and have a great day!