This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1473-Q1: CAN Transciver short to battery

Part Number: TCAN1473-Q1

Hi experts,

for the CAN transceiver we are using following ICs for our project.

TCAN1473CDMTRQ1 for the wakeup CAN and TCAN1472VDRBRQ1 for the ones without wakeup.

As you know we have the Req. Short circuit to battery at CAN-High and CAN-Low.

The test says:

We must apply 52V for 60s on CAN-High and on CAN-Low.

 

From the datasheet of the Transceivers both have these values:

can spec for e2e.png

 

Its only specified up to 40V do you have a value up to 52V?

If the sinking current is the same for 52V as for 40V we would have a power loss in the transceiver IC of 0,115A*52V = 5,98 W for 60s. Does the transceiver survive this? Or did I overlook some safety shut off?

Thanks and best regards,

Michael