Part Number: TCAN1473-Q1
Hello experts,
for the CAN transceiver we are using following ICs:
TCAN1473CDMTRQ1 for the wakeup CAN and TCAN1472VDRBRQ1 for the ones without wakeup.
As you know we have the Req. Short circuit to battery at CAN-High and CAN-Low.
The test says:
We must apply 52V for 60s on CAN-High and on CAN-Low.
From the datasheet of the Transceivers both have these values:

Its only specified up to 40V do you have a value up to 52V?
If the sinking current is the same for 52V as for 40V we would have a power loss in the transceiver IC of 0,115A*52V = 5,98 W for 60s. Does the transceiver survive this? Or did I overlook some safety shut off?
Thanks and best regards,
Michael