Part Number: SN65DSI83

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DSI83

Hi Hailei,
If the device ADDR pin is connected to 1.8V rail, the address will be 0x2D. If it is connected to directly to ground, the address will be 0x2C. Note that these are 7-bit addresses.
Is the controller successfully reading/writing the registers with the 0x2C address? You could also try it connecting directly to ground by replacing the ADDR 1kOhm resistor with a 0-Ohm resistor.
Best regards,
Ikram