This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIC10024-Q1: TIC10024QDCPRQ1 comparator detection time vs Maxim's input deglitch

Part Number: TIC10024-Q1

Dear team,

Could you please provide feedback to questions below? Thanks:

"

We have some doubts about the contact monitor, let me give you some background before jumping to the questions.

We were using the CM from Maxim (MAX20091ATM) in the past, with which we were having misreading input issues at low temperatures (-40deg). Studying the route cause, we realize that Maxim CM has a “deglitching” strategy that is a time delay to filter possible glitches that all CM inputs have. This delay plus the one that input capacitance adds to total reading time may compromise the correct open switch reading at polling mode (the only current that charge the external capacitance is the wetting current).

  

With that said, we want to understand what is the maximum delay that TIC10024QDCPRQ1 has at its inputs at worst case conditions. From datasheet, we only see “comparator detection time” with nominal value = 18us.

  

The questions are:

  • What is exactly the “comparator detection time”?
  • Is there any “deglitching” strategy at CM inputs?
  • What is the maximum delay time that the CM adds to the total reading time under worst case conditions? I am referring to the maximum delay time from when the input voltage level reaches the programmed threshold until this event is reported.

"

Rgds, Jose