Part Number: DP83TC817S-Q1
I've tried to clock the "PTP Reference Clock" as stated in <SNLS779A – JULY 2025 – REVISED NOVEMBER 2025>.
To change PTP_PLL to 125MHz: Writing 0x6666 to ref D35h and D36h - OK after both writes performad.
Set clock reference to PTP_PLL with 8ns step: Writing 0x1088 to ref D27h - OK.
Staring the clock: Writing 0x0004 to ref D00h - OK.
Reading clock value every second: as per page 36 7.3.1.1.2.1 "Read a time value"
Now, the clock increases twice like the increment happens on a 250MHz basis.
AM I missing something?
On a side note: I would like to bring this clock uot to the controler, Is that possible?