Part Number: DS125DF111
Other Parts Discussed in Thread: DS110DF111
Hi Support Team,
I am designing a product that requires a 10G network interface. My design includes a SoC with a 10G XFI interface, which I would like to connect to an SFP+ module. After researching online, I found that a retimer is needed between the SoC and the SFP+ module to ensure a reliable connection, resulting in the following topology:
SoC ------------- Retimer -------------SFP+ module
The DS125DF111 appears to meet my requirements for this role. However, this solution raises several questions I would like to clarify:
- Connection topology. Does the architecture above (SoC ------ Retimer ------ SFP+ module) seem correct? Are there any drawbacks to this approach? Is the DS125DF111 a suitable retimer for this application, or would you recommend an alternative?
- Retimer configuration. The XFI interface of my SoC operates at a fixed data rate of 10.3125 Gbps, which falls within the DS125DF111's supported range of 9.8–12.5 Gbps. Do the default register settings support this data rate out of the box, or is manual configuration required?
- Configuration tooling. I can see there is no dedicated driver for the DS125DF111. I did find a reference to the SigCon Architect 3.0.0.10 tool, which appears to support DS125DF111 configuration and monitoring. Is this tool still the recommended option? It appears to be approximately six years old — has TI released a more recent version?
- EEPROM programming. The DS125DF111 datasheet mentions the ability to automatically upload configuration data from an external EEPROM IC. Can SigCon Architect be used for EEPROM programming? Additionally, what I2C address should be assigned to the EEPROM IC? I was unable to find this information in the datasheet.
Thank you in advance for your assistance.