This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS25CP102: Can AC-coupled input common-mode near 0 V cause device damage?

Part Number: DS25CP102
Other Parts Discussed in Thread: LMH0344, , DS25CP104A

Hi TI team,

I have a follow-up question about DS25CP102TSQ input biasing when AC coupling is used.

I referred to these previous E2E threads:

Based on this, I understand that AC coupling without external bias is not a recommended operating condition.

My question is about the following case:

  • AC coupling is used

  • no external bias is added

  • the input common-mode is therefore near 0 V

  • each input pin voltage still remains within the Absolute Maximum Rating for LVDS Input Voltage (-0.3 V to +4 V)

In this condition, can this cause physical damage to the DS25CP102TSQ device itself?

Or should this be understood only as a functional/specification issue, meaning that correct operation is not guaranteed, but device damage is not expected as long as the Absolute Maximum Rating is not violated?

I would appreciate TI’s clarification on whether this condition should be treated as:

  1. operation not guaranteed only, or

  2. possible device damage risk.

Best regards,
Diego