This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: SN65DSI86 hardware questions

Part Number: SN65DSI86

Hi Team,

Regard SN65DSI86, Customer want to know if we can support below requirements:


Source Bus type:4lane MIPI C/DPHY 2.5Gbps;
Source terminal number:1.0;
Sink Bus type:4lane DP1.2 or DP1.4 support 4K30;
Sink Terminal number:1.0;
Support Lane swap:Yes; (Type-C output, will plug-in forward and backward)

Thank you,

Yishan Chen

  • Hi Yishan,

    Resolution:

    The SN65DSI86 converts DSI input to eDP output. It can support D-PHY only, up to 1.5 Gbps per lane for a maximum of 12 Gbps video bandwidth, as mentioned in the datasheet.

    It can support eDP 1.4, and the maximum DP rate per lane is 5.4Gbps.

    The 4K30 resolution bandwidth will depend on the exact PCLK used.

    As an estimate, if the pixel clock rate for 4K video at 30 fps is ~297 MHz, then the video bandwidth required will be = pclk * bpp = 297MHz * 24bpp = 7.128 Gbps. This should be supported since it is below the 12 Gbps DSI limit.

    Lane swap:

    The device also support lane swapping using the 0x59 register.

    DP Alt-mode and Type-C:

    For using DP output with Type-C, DP Alt-mode will need to be used with a suitable separate PD controller device, and type-C redriver such as TUSB546A. 


    Best regards,
    Ikram

  • Hi Ikram,

    Thank you for your quick response.

    Two more questions to check the detail:

    1) Only support eDP1.4 or device can also support original DP1.2/1.4, I see from some posts that SN65DSI86 can also compatible to DP1.4?

    2) Are Lane swap and DP Alt mode are two differnt concepts? By using Lane Swap they can support type-C double-side plug in, but for the protocol, they still need chip to support.

    Thank you,

    Yishan Chen

  • Hi Yishan,

    1. Yes this device can also support DisplayPort interface. The hardware and software configurations have to be done differently for DP applications.

    There are some details shared in this E2E thread: SN65DSI86-Q1: Driving a display port connector instead of eDP


    2. Could you tell us what you mean by lane swap. In my previous response, by lane swap I was referring to changing the output lane assignments for the pins.


    For using DP output with Type-C, DP Alt-mode will need to be used with a suitable separate PD controller device, and type-C redriver such as TUSB546A. 

    Additional components will be required for type-C connection for DP alt-mode. You can consider using the TUSB546A if it works for your application.


    Best regards,
    Ikram