Part Number: TSER953
Other Parts Discussed in Thread: DS90UB960-Q1, DS90UB953-Q1, DS90UB960-Q1EVM
Hi There,
We are using the DS90UB953-Q1 Serializer on our camera board and the DS90UB960-Q1 Deserializer on the carrier board. The FPD-Link III connection is configured in synchronous mode with a 50 Mbps back-channel rate, and Adaptive EQ is enabled.
We occasionally observe link errors in the logs (CRC error details attached here: Error_Ser_Deser.docx ), including both correctable (corr) and uncorrectable (uncorr) errors. To investigate, we performed a link margin analysis. The results indicate that the expected criteria of 4 strobe and 3 EQ green boxes are met (refer to the example image below). However, the link still appears to be somewhat sensitive.

Could you please advise if there is any method to fine-tune the back-channel clock for improved stability? Additionally, are there any undocumented or unexposed registers in the serializer or deserializer that could help optimize this behavior?