This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: DS90UB948-Q1 schematic design check

Part Number: DS90UB948-Q1

Dear team,

The attachment is a schematic diagram of the application of DS90UB948-Q1 Single coaxial signal input, video resolution of 1920 * 1080. Dual LVDS output Please help check if the configuration in the schematic is correct There are two other questions: First, in coaxial signal input, does GND need to add TVS, and if so, at which position? Secondly, regarding BISTEN and BISTEC, if they are not connected to the MCU, can they be configured according to the schematic diagram

Best,

Jim

DS90UB948Q1_SCH.pdf