Part Number: TXE8116
Hi team,
I am planning to use TXE8116 and would like to input a signal from a photocoupler.
My understanding is that a photocoupler is a relatively slow device in terms of signal transition speed.
In this case, is it acceptable to directly connect the output of the photocoupler to the TXE8116 input?
In this case, is it acceptable to directly connect the output of the photocoupler to the TXE8116 input?
Specifically, I would like to confirm the following:
- Can TXE8116 correctly recognize slow rise and fall times from devices such as photocouplers?
- Are there any concerns or limitations when directly interfacing a slow device like a photocoupler?
Best Regards,
Shota
Shota