This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XIO2001: CLK6 Feedback Length on a Module Design

Part Number: XIO2001

Hello,

We're developing a card which is part of a system in wich there is a module (controller) containing the XIO2001 bridge and it is connected on a backplane with other 5 modules (peripherals).

The XIO2001 clock outputs are routed on the controller from the bridge to the connector with low skew.

Through the backplane, the point-to-point clocks are routed to all the modules with low skew, and inside the peripheral modules, the clock lengths are all the same.

The question that rises is the following: 

  • What shall be the feedback from CLK6 to CLK pin in the controller module in this case?

Thanks!

 

Best regards,

Diego.