Part Number: TUSB216
How are the gain's set by the chip? Is there a Lead/Lag compensator built into the IC to help provide the boost needed?
Would it be possible to further "Tune" the values to an inbetween stage, or do the resistances provided for the gain need to be within a certain tolerance around the values stated in the datasheet/on the EVM? (EX: Would Rboost set to 5.1K provide a boost level that would fall between boost levels 2 and 3?)
Are there On-Die Resistors that the IC enables/disables by using I2C control?
How much do temperature swings affect the performance of the gain?
Do we need to characterize the gain if the IC will live in an enclosure that stays around 40C nominally?
What happens when you have a high gain setting via hardware and then attempt to use the lower gain settings via I2C? Would it default to the highest gain?