Part Number: DS110DF111
Hi everyone,
I'm designing a 10G OEO retimer board based on the DS110DF111 and encountered a signal polarity challenge.
Background:
- The SFP+ Module's RX signal needs to be fed into the DS110DF111's INA/INB for signal regeneration
- Due to PCB layout constraints, I had to reverse-connect my Channel A input signal (RX+ to INA-, RX- to INA+)
- The output end also needs to be inverted to match the downstream device's expectation
Question:
According to Datasheet section 7.5.1.19, Register 0x1F bit 7 can only invert output polarity. I could not find a register to control input polarity inversion.
Please advise:
- Is there a register available to invert input polarity?
- If not, can I reverse the connections on the PCB + only invert the output via software (0x1F bit 7 = 1), so the two inversions cancel out? Will the CDR still lock properly on the reversed input signal?
- Are there any alternative recommended solutions?
Thanks for your insights!
Kind regards,
Nanjun