Part Number: TMDS1204
Hi Team,
I am facing issue while testing HDMI 2.1 TX.
The TMDS is set in I2C mode and all the side band signals are floating ex:CTLEMAP_SEL, LINEAR_EN, MODE, AC_EN, TXPRE, EQ1, TXSWG, only EQ0 is pulled high so that I2C address will be 5B.
We are testing 4k @60 fps and running in bare metal selecting 4 lanes at 8 Gbps we get the sink info saying 4th lane as invalid, but the test pattern will be generated.
We tested multiple resolution but the 4th lane is still invalid for all resolutions and when we run 4k @120 fps the 4th lane is still invalid as before but there will be no output on the monitor.
Please help us debug this issue and bring up the 4th lane.
I have attached schematics.
I have also attached the logs below, in which you can see the logs for 1080p @ 60 , 4k @ 60 and 4K@ 120, the 4th lane is still invalid but output TPG(Test pattern) is there for only for 1080 and 4k 60 but no output for 4k 120 we can see the video lock in FPGA which staes there is output from FPGA which is input to the IC.
hdmi_2p1.txt