Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS110DF1610: request a BSDL for DS110DF1610

Part Number: DS110DF1610
Other Parts Discussed in Thread: DS125DF1610

hi,I'm urgency need DS110DF1610 BSDL file for JTAG test . Does DS110DF1610 and DF125DF1610 compatible for BSDL ?

  • Hi Zheng,

    You can find DS125DF1610 programming guide at link below, which contains BSDL file.  These are very similar devices, so I would expect BSDL to be very similar, if not the same.  We don't have separate DS110DF1610 BSDL file.

     DS125DF1610EVM: Interface forum 

    Thanks,

    Drew

  • Hi Drew

    thank you for your quickly reply,

    i have use the BSDL DS125DF1610 but found the Differential signal TX and RX define in BSDL all is "O" -output , see the load BSDL behavior as below  .

     

  • Hi Zheng,

    Can you clarify how you are seeing RX listed as output?  I just see TX listed as output in the file.  It appears RX is input.

     RX_0A_P, RX_0A_N, RX_0B_P, RX_0B_N, RX_1A_P, RX_1A_N, RX_1B_P, RX_1B_N :
    in bit;
     RX_2A_P, RX_2A_N, RX_2B_P, RX_2B_N, RX_3A_P, RX_3A_N, RX_3B_P, RX_3B_N :
    in bit;
     RX_4A_P, RX_4A_N, RX_4B_P, RX_4B_N, RX_5A_P, RX_5A_N, RX_5B_P, RX_5B_N :
    in bit;
     RX_6A_P, RX_6A_N, RX_6B_P, RX_6B_N, RX_7A_P, RX_7A_N, RX_7B_P, RX_7B_N :
    in bit;

     "61 (AC_2, TX_1A_P, OUTPUT2, X)," &
     "60 (AC_2, TX_0B_P, OUTPUT2, X)," &
     "59 (AC_2, TX_0A_P, OUTPUT2, X)," &
     "58 (AC_2, TX_2A_P, OUTPUT2, X)," &
     "57 (AC_2, TX_1B_P, OUTPUT2, X)," &
     "56 (AC_2, TX_3A_P, OUTPUT2, X)," &
     "55 (AC_2, TX_2B_P, OUTPUT2, X)," &
     "54 (AC_2, TX_4A_P, OUTPUT2, X)," &
     "53 (AC_2, TX_3B_P, OUTPUT2, X)," &
     "52 (AC_2, TX_4B_P, OUTPUT2, X)," &
     "51 (AC_2, TX_5A_P, OUTPUT2, X)," &
     "50 (AC_2, TX_5B_P, OUTPUT2, X)," &
     "49 (AC_2, TX_6A_P, OUTPUT2, X)," &
     "48 (AC_2, TX_6B_P, OUTPUT2, X)," &
     "47 (AC_2, TX_7A_P, OUTPUT2, X)," &
     "46 (AC_2, TX_7B_P, OUTPUT2, X)," &

    Thanks,

    Drew