Part Number: DP83867CR
Hi,
We are using the DP83867CRRGZ on our custom board, but the Ethernet link does not come up when connected to a PC.
Current status:
- The 25 MHz clock is present at the XI pin.
- RESET_N and INT_PWDN are pulled up to 3.3 V.
- The PHY registers can be accessed through MDC/MDIO from Linux.
- The firmware is based on software that worked on a TI evaluation board.
- The PHY link status remains down.
The attached PDF contains:
- P1: Circuit schematic
- P2: 25 MHz clock waveform at the XI pin
Could you please review the attached schematic and advise on the following?
1. Is there any hardware issue that could prevent link-up?
2. Is it correct to leave VDDA1P8 pins 13 and 48 unconnected?
3. Is any additional register configuration required for this custom board?
Device: DP83867CRRGZ
MAC interface: RGMII
MagJack: HFJ11-1G41E-L12RL
Best regards,
Conor