DS160PT801X16EVM: Accessing retimer EEPROM

Part Number: DS160PT801X16EVM
Other Parts Discussed in Thread: DS160PT801

Hi,

Is there any EEPROM configuration file for gen4 x8 PCIe. Is it possible to access and configure the EEPROM directly through the I2C interface or any other interfaces without using the Texas Instruments SigCon Architect EVM GUI? If so, could you please guide us through the procedure for accessing and configuring the EEPROM via I2C? It would also be helpful if you could share the corresponding EEPROM configuration file, if available.

Thanks and Regards.

  • Hi,

    1. You can generate new EEPROM file by loading an existing file. Then adjusting share register address 0xF3[4:0]. For x8, set 0xF3[4:0] = 0x1. 

    2. You can use a 3rd party host adapter like aardvark to flash the eeprom instead of SigCon architect GUI. 

    Best,

    Charles

  • Hi Charles,

    Thankyou for your response. 

    We have connected PCIe retimer to RFSoC I2C(master), please find the attached BD. So, we want to program the retimer EEPROM via retimer SMB interface. So, could you please let us know, how to program retimer EEPROM via Retimer SMB without any other adapter. We are planning to program it through baremetal applicaiton running on RFSoC device. So could you guide us how the programming can be done.

    Regards,
    Vishnuram

  • Hi Vishnuram,

    Understood. Please see section 3.1 EEPROM Write in the DS160PT801 EEPROM Configuration Guide. 

    Best,

    Charles