Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding tlk2218 -8 port GIGA\BIT ethernet transceiver - Hardware

7607.Gigabit -Ehernet.doc

Hi,

 I'm working on 8 channel AV encoded output over IP. Each video encoder card provide video over Ethernet. The Encoder doesnot have integrated phy and hence using separate Phy. There is a requirement to combine all 8 outputs to single via one RJ45.

Planning to interface all encoded MII interface of all 8 boards to the 8 port GIGABIT Ethernet transceiver tlk2218and then the ouput is to be connected to RJ45 via magnetic.Attached the general block diagram

Let me the proposed design works out.

Thanks,

Sangeetha