Other Parts Discussed in Thread: TCA9517
My customer wants to make VOL small using TCA9517.
Is TCA9517 usable by the circuit of page2 of the attached file ?
And, is TCA9517 usable by the circuit of page3 of the attached file?
please give me advice.
<My guess>
I think that the circuit of page2 is usable.
=>datasheet P9 “Master devices can be placed on either bus.”
I think that the circuit of page3 is not usable.
=>datasheet P2 “The TCA9517 cannot be connected B side to B side”
<Background>
By the usage of my customer, the SDA/SCL line has many noises.
(The noise is adverse effects of the cables.)
Therefore,The low level output voltage(VOL) of TAC9517 may become higher than "Low level input voltage(VIL=0.99V)" of the Slave device.
(the circuit of page1 of the attached file)
So my customer intends to prevent the adverse effects of the noise by making VOL small.
・TCA9517 1chip Circuit VOL = 0.6V (attached file page1) => now
・TCA9517 1chip Circuit VOL = 0.2V (attached file page2) => in review 1 (My idea)
・TCA9517 2chip Circuit VOL = 0.2V (attached file page3) => in review 2 (My customer idea)
Regards,
Kanemaru