Hello,
I'm developing a board and I'm using the PCI2050B bridge connected to a FPGA V-6 as target and configuring the PCI Bridge through Power PC. PCI bridge is running in 33 MHz configuration both primary and secondary side. While communication with V-6 FPGA, when ever data is captured in Chip Scope it is not coming as as per spec, First address is coming,after that in place of valid data some junk type of address is coming after that only data is coming. Where as per spec after address valid data should appear.
For your reference snap shot of chip scope is attached
1157.New Microsoft Office Word Document.doc
Deepak