Other Parts Discussed in Thread: XIO2001, XIO2001EVM
Hi
I have some Application issue in TI XIO2001
Currently, we are debugging AT-2916SX PCI card issue on platform AmazonDT.
AT-2916SX web : http://www.alliedtelesis.com/media/datasheets/2916sx_ds.pdf
We use AT2916SX with onboard XIO2001 , we can not open system.
Let me describe the symptom I found on on-board PCI slot (connected to TI PCIe-to-PCI [XIO2001]) with AT-2916SX as following:
(Environment: BIOS does not assign Expansion ROM base address. I manually assign the address under runtime.)
1. After reading device option rom from offset 0x1f84~0x1f87, system will hang if we continues to perform some reading action on other locations.
2. Per item#1, after reading any byte from offset 0x1f84~0x1f87, reading other locations which their data are not 0xff will become 0xff as well.
With the PCIe-to-PCI add-on card[TI XIO2001 EVM], I found that PCI CMD register is sometimes cleared after we enable device decode.
It causes option rom not dispatching and no PXE boot capability.
Observed this symptom on other platforms as well.
Did you have any experience/suggestion about these symptoms? The register setting in attachment File [ on board and EVM ]