Other Parts Discussed in Thread: TCA9406
Hello,
My customer has some questions about PCA9406.
[Q1] Please refer to an attached file.
[Q2] Please refer to an attached file.
Regards,
Hiroshi Katsunaga
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TCA9406
Hello,
My customer has some questions about PCA9406.
[Q1] Please refer to an attached file.
[Q2] Please refer to an attached file.
Regards,
Hiroshi Katsunaga
Katsunaga-san,
First of all, I believe you mean TCA9406. TI does not offer a PCA9406 device.
[Q1] Yes, the device can support your proposed circuit. See page 9 of the datasheet: "One advantage of the TCA9406 translator is that either power supply can be ramped up first. Another advantage is that either power supply can be set to 0 V, and the outputs are in high-impedance state."
[Q2] Footnote 3 is only applicable when both VCCA and VCCB are powered. I would suggest following the suggested design for the OE pin, also from page 9 of the datasheet: "A pulldown resistor tying OE to ground should be used to ensure that bus contention, excessive currents, or oscillations do not occur during power up and power down"
Thanks,
Brian
Hi Brian-san,
Thank you for answering my question.
I'm sorry, my questions meant TCA9406.
I understood your comment.
Best Regards,
Hiroshi Katsunaga