This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26LV31E/32E / evaluation results



Hi,

I post another E2E, and I have got AM26LV31E-Evaluation.pptx.

8738.AM26LV31E Evaluation.pptx

The test signal is a10MHz 50% duty cycle clock.

Is there evaluation results of 20MHz 50% duty cycle clock?

Best Regards,

Kato

  • Kato-san,

    I do not have that data, but it can be visualized by looking at the 10MHz wave forms.
    Because the pulse has settled half way though the bit time the waveform would be the same expect visualize the the last half of the pulse was not there.

    For the other question about 100ft (30 meters) and 20Mbps, it is clear that the pulse doesn't settle fully until the end of the 25nS pulse so a random bit pattern will have significant jitter.