Other Parts Discussed in Thread: ISO1540
Hi All,
Now our customer has evaluated ISO1540 on their prototype, but then they confirm the abnormal behavior. Output CLK from SCL2 is skipped though CLK is input to SCL1 correctly. This behavior is confirmed when the load current at DC/DC converter on the same board is heavy, so the VCC or GND line may be noisy.
Please see the waveform below.
5875.ISO1540 pulse sikipping.pdf
[Question]
Is it possible that the noise on VCC or GND will be the cause of such pulse skip?
Your advice will be appreciated.
Best Regards,
Sonoki / Japan Disty