Other Parts Discussed in Thread: XIO2001
Hello.
I'm doing design "PCIe to PCI raiser card".
I choose "XIO2001".
Only need 1 channel PCI and then I don't need "-12V"
Q1) Someone review my schemetic?
Q2) To see "TI EVM circuit", between "REF0_PCIE" and "REF1_PCIE" pins is connected 14.532Kohm(1%)
But 14.532Kohm is not available in my side, so I take 15Kohm(5%) instead.
I’m likely to understand why TI recommends 14.532(1%). Is it a problem if 15K is substitute for 14.532K?
-> here is my schemetic