Other Parts Discussed in Thread: DS90UB913A-Q1, DS90UB914A-Q1
Hello,
Please see the attached file.
Our customer use Imager which have SPI I/F and they use the MCU for bridge the SPI to I2C.
Current ly, they can't read the imager data.
Please see the attached file.
The DS90UB913A-Q1 sent the ACK when receive the address data and Read bit.
However, the data was not sent to Des due to the data of imager was not ready.
Thus, SCL of Ser was held to Low until the data ready.
After the data ready, SCL of Ser is asserted to high but the data is not trasmitted due to there is no SCL.
Could you please let me know this reason?
Should DS90UB913A-Q1(slave) output the SCL and SDA without SCL from DS90UB914A-Q1(master)?
Best Regards,
Ryuji Asaka